Part Number: DP83867IR
Tool/software:
application scenario:IOT device
Soc platform:NXP imx8mm, dp 83867 is used on this SOC, linux system
I could connect to my host PC when the ethernet cable connected between PC and our device.
The problem is after unplug the cable and leave my device running for one or two days, then I could not connect to my host PC after I plug in the ethernet cable.
I read the phy register 0x1, it showed 0x7969. It means the autonegotiation is complete while the valid link is not established.
recover method:
ifconfig eth0 down and up to reconnect the phy
How does this happen when auto-negotiation is finished while the link is not established? Could you help investigate?