Tool/software:
When using ti960+ti953, connect sensor ov-xxx, during stability test, randomly encounter once whole ti960+ti953+sensor start, no mipi packed received from ISP, and sensor streaming register 0x100 =1(means streaming) serdes status register dumped as below;
(and found difference between normal streaming and no frame
ti-2 rx_port 0, ti953 [0x53 0x9] when no frame, normal this value is 0x00,
)
ti-2 rx_port 0, ti953 [0x52 0x45]
ti-2 rx_port 0, ti953 [0x53 0x9] 
ti-2 rx_port 0, ti953 [0x55 0x0]
ti-2 rx_port 0, ti953 [0x56 0x0]
ti-2 rx_port 0, ti953 [0x57 0x0]
ti-2 rx_port 0, ti953 [0x58 0x7]
ti-2 rx_port 0, ti953 [0x59 0x7]
ti-2 rx_port 0, ti953 [0x5a 0x7]
ti-2 rx_port 0, ti953 [0x5c 0xff]
ti-2 rx_port 0, ti953 [0x5d 0x0]
ti-2 rx_port 0, ti953 [0x5e 0x64]
ti-2 rx_port 0, ti953 [0x5f 0x0]
ti-2 rx_port 0, ti953 [0x60 0x0]
rx_port 0, ti953 csi payload [0x62 0x12]
rx_port 0, ti953 csi payload [0x63 0xd0]
rx_port 0, ti953 csi payload [0x65 0x7]
rx_port 0, ti953 csi payload [0x66 0xf]
ti-2 rx_port 0, ti960 [0x51 0x0]
ti-2 rx_port 0, ti960 [0x52 0x0]
ti-2 rx_port 0, ti960 [0x53 0x3]
ti-2 rx_port 0, ti960 [0x54 0x2]
ti-2 rx_port 0, ti960 [0x59 0x0]
ti-2 rx_port 0, ti960 [0x5a 0x0]
ti-2 rx_port 0, ti960 [0x5b 0x30]
ti-2 rx_port 0, ti960 [0x4d 0x13]
ti-2 rx_port 0, ti960 [0x4e 0x4]
ti-2 rx_port 0, ti960 [0x55 0x0]
ti-2 rx_port 0, ti960 [0x56 0x0]
ti-2 rx_port 0, ti960 [0x4f 0x64]
ti-2 rx_port 0, ti960 [0x50 0x0]
ti-2 rx_port 0, ti960 [0x73 0x0]
ti-2 rx_port 0, ti960 [0x74 0x0]
ti-2 rx_port 0, ti960 [0x75 0x0]
ti-2 rx_port 0, ti960 [0x76 0x0]
ti-2 rx_port 0, ti960 [0xe 0x1]