Part Number: DS90UB953A-Q1
We checked CSI error and PASS error in 4 patterns( Continuous Clock mode and Non-Continuous Clock mode On sensor and 953A) .
Please refer attached xlsx files.
I have some questions below.
Q1) CSI errors were only observed on Pattern③ (Sensor :Non-Continuous clock setting /953A :Continuous clock setting ) .
954 addr0x4E (RX_PORT_STS2 ) Read data: 0x4D (CSI_ERROR=1)
954 addr0x7A (CSI_RX_STS ) Read data: 0x02 (ECC2_ERR=1)
But after a few ms the CIS error disappears. Does it have the function to recover from CSI errors on 953A-954 system?
Q2) CSI errors could not observed on Pattern② (Sensor :Continuous clock setting /953A :Non-Continuous clock setting ) .
The behavior is the same as Pattern ① (Sensor :Continuous clock setting /953A :Continuous clock setting ) .
Why doesn't errors occur even though the clock mode settings are different between the sensor and 953A?
Q3) The following alarm will be obseved to the addresses 4D and 4E of 954 after the initial setting.
954 addr0x4E (RX_PORT_STS2 ) Read data: 0x45 (LINE_LEN_CHG=1/LINE_CNT_CHG=1)
Let me check if the behavior is correct.
Marge Sens_Ser Conti_NonConti.xlsx
I'm looking forward your reply.