Part Number: TFP410
Other Parts Discussed in Thread: TFP403
Tool/software:
Hello E2E Experts,
Good day.
In reference to the abovementioned E2E post, our clock frequency is going to be significantly lower then 25MHz. It’s at 7,7MHz.--which is unfortunate.
However that leaves me with another question.
So from my understanding the TFP410 will not be able to produce a DVI compliant signal if it is fed a clock frequency that low.
Will the chip still produce a signal that is just not compliant with the DVI specs though? Meaning with a clock that is below specification or is it going to produce no signal at all?
Additionally, I have found a similar question regarding the TFP403:
What if input pixel clock frequency is less than 25MHz for TFP403?
I guess these chips have some margin. I might be able to tweak the receiving end to accept a non DVI compliant signal.
Regards,
TI-CSC