Tool/software:
Maximum reflow cycle for the Components
TCAL9539RTWR, TPS7A1412PDRVR, OPA328DBVR, INA310A3IDGKR, REF4132B25DBVR, F28386DPTPS, PCA9306DCUR
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Maximum reflow cycle for the Components
TCAL9539RTWR, TPS7A1412PDRVR, OPA328DBVR, INA310A3IDGKR, REF4132B25DBVR, F28386DPTPS, PCA9306DCUR
Hi Jeya,
This device is specified as Level 1 MSL rating as per JEDEC industry standard with a maximum peak temperature of 260°C (+0° / -5°C).
Regards,
Tyler
Hi ,
Thanks for the response
Kindly share how many reflow cycle it can with stand for the mentioned parts
TCAL9539RTWR, TPS7A1412PDRVR, OPA328DBVR, INA310A3IDGKR, REF4132B25DBVR, F28386DPTPS, PCA9306DCUR
Regards
Jeya Dharani
Hi Jeya,
Please see this e2e thread:
For TCAL9539RTWR and PCA9306DCUR, both are MSL1, should be able to withstand 3 reflow cycles.
Thanks,
regards,
Tyler
Hi,
Thanks for the response
Could you share how many reflow cycle it can with stand for other parts too
TPS7A1412PDRVR, OPA328DBVR, INA310A3IDGKR, REF4132B25DBVR, F28386DPTPS
Hi Jeya,
My team does not support the other devices. You will have to ask the correct team according to each device for a direct answer.
However, based upon JEDEC standards for MSL1 ratings, I am assuming that the same # of reflow cycles would apply to the other devices if they are indeed MSL1 rated.
Regards,
Tyler