Other Parts Discussed in Thread: TCAN4550,
Tool/software:
Hi,
As a followup to the previous question, we are generating a clock from a small RISC-V processor, and want to know if the clock will be sufficient for a TCAN4551.
Summary of the system:
- We are planning on running the SPI at 16MHz (the fastest our SoC will run the SPI).
- We are planning on running the CAN bus at 125Kbps.
- We are now using the TCAN4551 instead of the TCAN4550 because of the 1.8V support.
Here's an oscope trace of the clock we are currently generating:

As you can see, the clock has some jitter, you see the min at 21.05MHz, and the max at 21.98MHz. The duty cycle varies a bit between 48.30% and 49.50%. We are working on reducing the jitter as much as possible, but don't know if we can get much better than this.
Will this clock be sufficient for the TCAN 4551 at 125Kbps CAN speeds?
Thank you!
Sandra