Part Number: TUSB212
Tool/software:
Hi, I want a clarification on the following.
Do we need to place EQ and DC_BOOST resistors, if we are using I2C mode?
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TUSB212
Tool/software:
Hi, I want a clarification on the following.
Do we need to place EQ and DC_BOOST resistors, if we are using I2C mode?
Thanks.
Hi Punsara,
For I2C mode, the initial setting for EQ and DC_BOOST is based on the resistor setup of those pins. So if you were to leave both the pins floating at device start-up/reset, you would start with EQ level 3, and DC_BOOST level mid. From there, you would be able to modify the values of these pins/registers via I2C.
Typically, we recommend keeping EQ at level 0 or 1, since level 3 can cause over-compensation or disconnects.
Please let me know if you have any other questions.
Thanks,
Ryan