Part Number: SIGCONARCHITECT
Other Parts Discussed in Thread: DS125DF1610, USB2ANY
Tool/software:
SigCon info:
Version:2.0.0.8
Build - 05/11/2016
Device: DS125DF1610
System info:
Windows 11 Pro
Version 10.0.22621 Build 22621
Python 3.9.8
Below is the content of error message window after I click from menu Script->Launch Window
Error 5000 occurred at Notifier Timed Out
Re-Driver Device GUI.lvlibp:GUI Wait for GUI Response via Notifier.vi:1:\Re-Driver Device GUI.lvlibp:Launch Macro Recording.vi\Re-Driver.lvlib:Main.vi
This error code is undefined. Undefined errors might occur for a number of reasons. For example, no one has provided a description for the code, or you might have wired a number that is not an error code to the error code input.
Additionally, undefined error codes might occur because the error relates to a third-party object, such as the operating system or ActiveX. For these third-party errors, you might be able to obtain a description of the error by searching the Web for the error code (5000) or for its hexadecimal representation (0x00001388).