Part Number: SN65DP141
Tool/software:
Hi Team,
Did we have guideline for SN65DP141 placement for 11 inch eRP cable?
If yes, could you share it with me? Thanks.
Regards,
Ben
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hey Ben,
What is an eRP cable, and do you have a sample loss profile for it? The DP141 is able to equalize up to 15dB at 6GHz (12Gbps). The placement of the DP141 should be placed at at the13dB loss point of the cable to provide 2dB of tolerance.
Hey Ben,
What is an eRP cable, and do you have a sample loss profile for it?
The DP141 is able to equalize up to 15dB at 6GHz (12Gbps). The placement of the DP141 should be placed at the13dB loss point of the cable to provide 2dB of tolerance.
Hi Vishesh,
I will check the cable with customer and based on the loss to recommend the placement. Thanks.