Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS100KR401: 10Gb Ethernet link random error

Part Number: DS100KR401
Other Parts Discussed in Thread: DS125BR401

Tool/software:

Hi Team,


            We are using DS100KR401SQE/NOPB in our design for 10G Ethernet links (Do not require link training ) from FPGA to SFP+ interface through back plane connections.

We set the redriver in limiting mode by connecting mode pin with 1K pull down resistor to GND. We connected SD_TH pin pull up to VDD through 1K resistor.

During 10G Link validation test we observed that link is getting up, But it creating errors randomly. We tried to optimize the link setting (VOD,EQ,DEM) of DS100KR401, but still we can not achieve the error free channels.

We tried to isolate the redriver by replacing other FPGA card that does not have redriver in the signal path. In these case we can able to achieve error free operation.

We tried to set the redriver in INB to OUTA loop back mode by writing 21 value in 0x02 register. Refer attached image for loop back operation. In this mode also we are getting random errors.

We tried to set the redriver in INA to OUTB loop back mode by writing 11 value in 0x02 register.In this mode we are getting error free channels.


Question 1: Can you please suggest what is the suggested setting for 10GbE interface in optical link(With out Auto Negotiation)?

Question 2: Whether (VOD,EQ,DEM)  setting applied during the redriver loop back operation also or these values will be ignored?

Question 3: How SI parameters handled during internal loop back operation inside redriver?

Thanks in advance,
Shenbagavalli.

  • Sl.No	Register Values
    1	0x02	31
    2	0x06	18
    3	0x2D	A9
    4	0x34	A9
    5	0x3B	A9
    6	0x42	A9
    7	0x10	A9
    8	0x17	A9
    9	0x1E	A9
    10	0x25	A9
    11	0x2E	00
    12	0x35	00
    13	0x3C	00
    14	0x43	00
    15	0x11	01
    16	0x18	01
    17	0x1F	01
    18	0x26	01
    19	0x2C	00
    20	0x33	00
    21	0x3A	00
    22	0x41	00
    23	0x0F	00
    24	0x16	00
    25	0x1D	00
    26	0x24	00
    

  • Hi Shenbagavalli,

    Is this related to the following thread?

    https://e2e.ti.com/support/interface-group/interface/f/interface-forum/1416538/ds125br401-ds125br401-10g-link-random-error-issue

    Can you clarify if DS100KR401 or DS125BR401 is being used?

    Best,

    Lucas