Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS125BR401: DS125BR401 : 10G Link random error issue

Part Number: DS125BR401
Other Parts Discussed in Thread: DS100KR401

Tool/software:

Hi Team,
            We are using DS125BR401SQE/NOPB in our design for 10G Ethernet links (Do not require link training ) from FPGA to SFP+ interface through back plane connections. We set the redriver in limiting mode by connecting mode pin with pull down resistor to GND.

During 10G Link validation test we observed that out link is getting up, But it creating errors randomly. We tried to optimize the link setting (VOD,EQ,DEM) of DS125BR401S, but still we can not achieve the error free channels.

We configured SD_TH in high state and we set the below mentioned signal detect registers for forcing forcing the Signal Detect function to be always ON.
0x0D[1]= 1'b, 0x14[1] = 1'b, 0x1B[1] = 1'b, 0x22[1] = 1'b
 0x2A[1]= 1'b, 0x31[1] = 1'b, 0x38[1] = 1'b, 0x3F[1] = 1'b

Observation 1:

We can able to achieve the error free channel while we set redriver during INB to OUTA loop back  mode by writing 21 value in 0x02 register.

We attached the current redriver register value for your reference. Refer attached image for loop back scheme diagram.

After validating back plane level loop back testing, we set 31 value in 0x02 register for normal operation in that case our link itself not active. So we programmed 50 value in 0x08 register & 20 value in register (0E,15,1C,23,2B,32,39 & 40) for idle control from registers to set output ON function.
In this case 10G link up but still we have random error.

Question 1: Can you please suggest what is the suggested setting for 10GbE interface in optical link(With out Auto Negotiation)?

Question 2: In 9.5.1.1.1 section of DS125BR401 data sheet mentioned that “This data loss can be eliminated by disabling automatic detection and forcing the Signal Detect function to be always ON”

How to disable the automatic detection in  DS125BR401?
What are register I need to overwrite for this operation?


Thanks in advance,
Esakki.

  • Sl.No	Register Values
    1	0x02	21
    2	0x06	18
    3	0x2D	A9
    4	0x34	A8
    5	0x3B	AB
    6	0x42	A9
    7	0x10	A8
    8	0x17	A8
    9	0x1E	A8
    10	0x25	A8
    11	0x2E	0
    12	0x35	0
    13	0x3C	0
    14	0x43	0
    15	0x11	0
    16	0x18	0
    17	0x1F	0
    18	0x26	0
    19	0x2C	0
    20	0x33	0
    21	0x3A	0
    22	0x41	0
    23	0x0F	0
    24	0x16	0
    25	0x1D	0
    26	0x24	0
    27	0x08	50
    28	0x01	0
    29	0x0D	2
    30	0x14	2
    31	0x1B 	2
    32	0x22	2
    33	0x2A	2
    34	0x31	2
    35	0x38	2
    36	0x3F	2
    37	0x0E	20
    38	0x15	20
    39	0x1C	20
    40	0x23	20
    41	0x2B	20
    42	0x32	20
    43	0x39	20
    44	0x40	20
    45	0x12 	0F
    46	0x19 	0F
    47	0x20 	0F
    48	0x27 	0F
    49	0x2F 	0F
    50	0x36	0F
    51	0x3D	0F
    52	0x44	0F
    

  • Hi Esakki,

    Which RX-detect setting are you currently using? For 10 GbE applications, manual RX-detect with input termination of 50 ohm should be used. This can be configured by pulling the RXDET pin high or programming 0x08[3]=1, 0x0E[3:2]=11, 0x15[3:2]=11, 0x1C[3:2]=11, 0x23[3:2]=11, 0x2B[3:2]=11, 0x32[3:2]=11, 0x39[3:2]=11, 0x40[3:2]=11.

    "Disabling automatic detection" refers to using manual RX-detect setting.

    Have you tried using loopback IN_A to OUT_B? I'm curious if this configuration resulted in no errors as well.

    Best,

    Lucas

  • Hi Lucas,
        We are using manual RX-detect with input termination of 50 ohm    option only. We already pulled RXDET pin high  through pull up resistor to VDD. So currently we set redriver in manual Rx- Detect settings only.
    We tried loop back in IN_A to OUT_B path, We can able to achieve the error free channel.

    We are facing issues while we set 0x31 data in 0x02 Address for normal operation.

    Question 1: Can you please suggest is there any other settings for 10GbE interface we need to program?

    Thanks in advance,
    Esakki.

  • Hi Esakki,

    Thank you for your feedback. I'd like to check, what testing was performed to optimize EQ, DEM, and VOD values? Optimizing these values is critical to error free operation. My recommendation is to optimize these values based on eye opening.

    1. Connect a high-speed sampling oscilloscope at the SFP port. Transmit PRBS data from the FPGA. Focus on one channel at a time, starting with EQ optimization.
    2. Start with minimum EQ setting and measure eye width/eye height on the oscilloscope. Step up the EQ, one index at a time, monitoring the eye width/eye height. Choose the optimal EQ setting based on maximum eye opening.
    3. Step through VOD and DEM values to optimize eye opening while maintaining the necessary peak-to-peak amplitude.
    4. Repeat steps 2-3 on the other 3 B channels.
    5. Is your FPGA able to measure diagnostics like eye width and eye height? Transmit PRBS data from the SFP port. Focus on one channel at a time, starting with EQ optimization.
    6. Repeat steps 2-3, focusing on each A channel one at a time.

    Additionally, is this E2E thread related? If this is the same project, can you clarify if DS125BR401 or DS100KR401 is being used?

    https://e2e.ti.com/support/interface-group/interface/f/interface-forum/1416885/ds100kr401-10gb-ethernet-link-random-error

    Best,

    Lucas