Other Parts Discussed in Thread: HD3SS3220
Tool/software:
Hi TI guru,
We perform USB compliance test on our board with TUSB1142 Redriver. (We used pin strap mode on TUSB1142.)
When we carry out USB compliance test, we fail on TD 7.31 Hot reset failure test with the failure message mention "The PUT without a captive re-timer doesn't transmit at least 16 polling LFPS bursts."
We perform some of the DOE, we remove TUSB1142 and connect it with jumper, by pass TUSB1142 and it able to pass the test.
USB compliance test FAIL with TUSB1142, we notice the electrical Idle duration was 6.528ms, and Rx.Detect ==> Polling LFPS only having 14/12 package.
USB compliance test PASS when we remove TUSB1142 and replace it with jumper (bypass), the electrical Idle duration was 142.024us, and Rx.Detect ==> Polling LFPS having 34/32 package.
What is going wrong here?
Thanks,
Best regards,
Alder