Part Number: TCAN1145-Q1
Other Parts Discussed in Thread: TCAN1044A-Q1
Tool/software:
Hi team,
I have some questions about the manual.
1.Which register does this reset refer to?FRAME_CNT_THRESHOLD(46H) or FRAME_CNTx(45H)?

2.Is the error counter mentioned in the manual (the default threshold is 31) the same register as the error counter (TEC/REC) that detects whether the node state has changed to error passive and bus off in ISO11898 ?

3.When the chip is in sleep-mode with WUF function enabled and VCC and VIO powered off, CAN Vsup be used only to detect CAN messages in WUF wake up and pull up INH?
4.In the wake up behavior configuration of RXD, the configuration of Toggle is different from that of pull-down. There is a tmode_slp_stby(yellow mask) and a tmode1(red mask). The tmode_slp_stby can be obtained according to the table in the manual. What is the tmode1 time length? What are the factors affecting it?


5.If RXD is configured to pull down wake-up, what is the waveform rule when it is held in stand-mode?(Flip once whenever the bus level duration exceeds twk_filter RXD?)
6.Regarding the scope of nINT, the manual says that nINT is the logic or of all errors in registers 8 'h50~8' h54 that do not mask.

However, it is also mentioned that the failure scope does not include VIO undervoltage, so in addition to VIO undervoltage, what other faults in 8 'h50~8' h54 are not included in the nINT interrupt scope? Or what register sets in 8 'h50 to 8' h54 will pull nINT down?

Best wishes