Tool/software:
Hello,
I openend this case some weeks ago, but unfortunately I could not make the measurement in time and case was closed after some days.
The original case was DP83867ERGZ-S-EVM: RFSoC (Ultrascale+) DP83867ERGZ-S-EVM Link Up but No Traffic (Ping)
I finally made a measurement, but the scope was 1GHz BW limited and the signals are very limited.
In this capture, the yellow corresponds to the diferential output of the evaluation board DP83867ERGZ-S-EVM (SO_P-SO_N). The green output is the output from the FPGA (PS-GTR3, GEM3).
The amplitud from the eval board seems to be ok, about 800mV over a differential impedance from 100Ohms. The amplitud from the RF-SoC seems to be ok, with a differential P-P amplitude of 1500mv aprox.
The register 0x0037 keeps on 0 value, which meas that the SGMII Autonegotiation was not done,
in U-BOOT
ZynqMP> mii write 0x00 0x0D 0x001F ZynqMP> mii write 0x00 0x0E 0x0037 ZynqMP> mii write 0x00 0x0D 0x401F ZynqMP> mii read 0x00 0x0E 0000
an in linux
Reg: 0x0000 Value: 0x1140 Reg: 0x0001 Value: 0x796D Reg: 0x0002 Value: 0x2000 Reg: 0x0003 Value: 0xA231 Reg: 0x0004 Value: 0x09E1 Reg: 0x0005 Value: 0xCDE1 Reg: 0x0006 Value: 0x006F Reg: 0x0007 Value: 0x2001 Reg: 0x0008 Value: 0x4006 Reg: 0x0009 Value: 0x0300 Reg: 0x000A Value: 0x3C00 Reg: 0x000D Value: 0x401F Reg: 0x000E Value: 0x1111 Reg: 0x000F Value: 0x3000 Reg: 0x0010 Value: 0x5848 Reg: 0x0011 Value: 0xAC02 Reg: 0x0012 Value: 0x0000 Reg: 0x0013 Value: 0x1C02 Reg: 0x0014 Value: 0x2BC7 Reg: 0x0015 Value: 0x0000 Reg: 0x0016 Value: 0x0000 Reg: 0x0017 Value: 0x0040 Reg: 0x0018 Value: 0x6150 Reg: 0x0019 Value: 0x4440 Reg: 0x001A Value: 0x0002 Reg: 0x001E Value: 0x0202 Reg: 0x001F Value: 0x0000 Reg: 0x0031 Value: 0x1111 Reg: 0x0032 Value: 0x00D3 Reg: 0x0033 Value: 0x0000 Reg: 0x0037 Value: 0x0000 Reg: 0x0043 Value: 0x07A0 Reg: 0x006E Value: 0x8820 Reg: 0x006F Value: 0x0110 Reg: 0x0086 Value: 0x0057 Reg: 0x00C6 Value: 0x0000 Reg: 0x00D3 Value: 0x0000 Reg: 0x00FE Value: 0xE721 Reg: 0x0134 Value: 0x1000 Reg: 0x0135 Value: 0x0000 Reg: 0x016F Value: 0x0015 Reg: 0x0170 Value: 0x0C12 Reg: 0x0172 Value: 0x0000 Reg: 0x01D5 Value: 0xF500
Autonegotiation from PHY is ok, and everything from PHY seems to be ok
root@sgmii:~# dmesg | grep macb [ 2.130847] macb ff0e0000.ethernet: Not enabling partial store and forward [ 2.147282] macb ff0e0000.ethernet eth0: Cadence GEM rev 0x50070106 at 0xff0e0000 irq 45 (00:0a:35:00:22:03) [ 7.663446] macb ff0e0000.ethernet eth0: PHY [ff0e0000.ethernet-ffffffff:00] driver [TI DP83867] (irq=POLL) [ 7.673253] macb ff0e0000.ethernet eth0: configuring for phy/sgmii link mode [ 7.685382] macb ff0e0000.ethernet: gem-ptp-timer ptp clock registered. [ 11.775311] macb ff0e0000.ethernet eth0: Link is Up - 1Gbps/Full - flow control tx
Maybe could you help me to find out why I can't get the link and auto-negotiation between GEM and PHY over SGMII?
Thanks a lot.