Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83561-SP: MAC Impedance RGMII

Part Number: DP83561-SP

Tool/software:

Hello,

For the impedance control, the 35 ohm recommended for RGMII in table 7-59 for MAC_IMPEDANCE_CTRL seems wrong in the specification and does not match the 50 ohm recommendation in 7.3.2 of 50ohms +/-20%.

Is 50 ohms correct and recommended? Do not understand the intent of the 35 ohm note.

Thanks!

  • Hi Tijana,

    Thank you for pointing out the 35Ω comment, I am unsure about the intent and will verify internally with my team, please allow me about a week to reach out and hear back. The guidance would be to keep the traces impedance matched to 50Ω, no series resistors are needed on the RGMII lines.

    Regards,

    Alvaro