Part Number: TLIN1029A-Q1
Tool/software:
Hello team,
Is it no problem when GND voltage is fluctuated from 0V <-> 2.0V (200Hz square wave) if the below table specs are satisfied?


Best regards,
Shotaro
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TLIN1029A-Q1
Tool/software:
Hello team,
Is it no problem when GND voltage is fluctuated from 0V <-> 2.0V (200Hz square wave) if the below table specs are satisfied?


Best regards,
Shotaro
Shotaro-san,
The LIN standard allows for GND shift up to 11.5% of VBAT (see ISO 17987-4 params 22-24). If the GND shift in your test is within this specification, then it should be acceptable. Outside of this range, you risk shifting the voltage references significantly enough to cause issues with the LIN duty cycle.
Keep in mind that this is part of the international standard for LIN, so these comments apply to all LIN transceivers across manufacturers.
If you are not using the LIN protocol, then it's certainly possible to communicate using a custom protocol that accounts for these timing differences. The transceiver will still interpret LIN signals as HIGH and LOW per the electrical characteristics in the data sheet.
Best,
Danny