Part Number: TPD1E6B06
Other Parts Discussed in Thread: ISO1044
Tool/software:
Hi,
I have connected the TVS Diode and Fuse with ISO1044 CAN for IC protection.
I want to confirm one point. Should the TVS Diodes (EC7, EC9, EC10) need to connect after the Fuse (RT7, RT9) as shown in the schematic shared (Connector---> Fuse---> TVS Diode---> TO ISO1044 IC) or Shall I need to connect the TVS Diode next to the connector and then to Fuse (Connector---> TVS Diode---> Fuse---> TO ISO1044 IC)?

Thanks