Part Number: TPD3S014
Tool/software:
Hello,
Some of our users have reported a chip burn with the TPD3S014DBVR.
They are using USB 2.0 devices, connected on the HOST port of our PCB.
Our design is supplying 5V (1A) on the host port, protected by the TPD3S014.
I received the products back for the maintenance, and indeed, I can see that the TPD3S014 is burn, and not providing the +5V output anymore (the +5V input, supplied internally on our design by a regulator, is still working).
Unfortunately, I can't reproduce the issue, it's rare but happen with some users.
Any ideas of how this issue can happen? For example, do you think an input supply voltage >5.5V can damage the TPD3S014?
Thanks a lot!
Jean