Part Number: TCA9539
Other Parts Discussed in Thread: PCF8574, TCA9554, TCA9554A, TCA9555, PCF8574A, PCA9554A, PCA9555, PCA9554, PCF8575
Tool/software:
Hi,
Would you please hlep review below TCA9539 schematic? thanks!
Jeff
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Jeff,
I am reviewing a total of 4 IO expanders in the schematic provided. Let me know if I missed anything.
|
U1 / U2 / U3 / U4 |
|
|
|
Check |
Status (good, bad, okay, ?) |
Comment |
|
Local Decoupling Capacitors |
U1: 100 nF, Good U2: 100 nF, Good U3: 100 nF, Good U4: 100 nF, Good |
Generally, a 0.1-uF capacitor is placed on VCC, as close to the device as possible |
|
Verify the schematic pinout matches the data sheet pinout |
U1: Good U2: Good U3: Good U4: Good |
|
|
Check that the pullup resistors are present on the SDA and SCL net within the schematic. |
U1: Verify U2: Verify U3: Verify U4: Verify |
I can't find them on the schematic, probably on another page. |
|
Unused GPIO pins are biased to either VCC or GND via resistor |
U1: Verify U2: Verify U3: Verify U4: Verify |
Most of TI's IO expander portfolio do not include internal pull-up resistors on the p-port pins; the exceptions are PCF8575, PCF8574, PCF8574A, TCA9555|PCA9555, PCA9554|TCA9554, and TCA9554A|PCA9554A and therefore can be left floating. An alternative approach is after powering up the device, any unused p-port pins can be set as an output (does not matter if set high or low). Need to verify what is the purpose of each GPIO. Follow the above description if the pin is going to be left as a floating input. |
|
Device address is unique on the bus unless using an I2C switch or I2C MUX to resolve conflicts |
U1: Good U2: Good U3: Good U4: Good |
All I2C addresses are unique between all TCA9539's |
|
If the device has a /RESET pin, bias the pin high (preferably with a pull-up resistor) after powering up. |
U1: Good U2: Good U3: Good U4: Good |
All pulled high through 0 ohm resistor |
|
If the device has a /INT pin and the /INT pin is used, tie this pin to a pull-up resistor. |
U1: Verify U2: Verify U3: Verify U4: Verify |
Need to verify if a pull-up resistor is provided on /INT. This is an open-drain output. |
Regards,
Tyler