Part Number: DP83867IR
Tool/software:
Hi Team,
One of my customer is considering DP83867IRRGZ for their upcomming project. They have riased below queries, kindly help with the response.
They are considering the DP83867IRRGZ Ethernet PHYs as a strong contender for their upcoming 1Gbps application in Communication interface devices and plan to proceed with an RGMII interface. Could you please confirm whether these parts support auto-negotiation with the RGMII interface, particularly given that the master module we will be interfacing with operates at only 100Mbps? Additionally, please confirm the auto-negotiation capabilities in terms of duplex mode (both full and half duplex).
Pls. help on below queries too.
- Do VDD1P0 is an Analog Supply or Not. Our understanding is it is an analog Supply
- Any risk in sharing same MDO Signal from FPGA to two PHY's (Both PHY's are DP83867IRRGZ)
- Any risk in sharing same MDIC Signal from FPGA to two PHY's (Both PHY's are DP83867IRRGZ)
- What is the purpose of the CLK_OUT. What could be the impact if it kept floated for 1Gbps.
- If JTAG Pins are not using, is it okay to Pull up JTAG_TDO, JTAG_TMS,JTAG_TDI and Pull Down JTAG_CLK
- INT / PWDN Pin Status : During Interrupt is the Pin acting as Output or Input
Regards,
Mitesh