Part Number: DS90UB947-Q1
Other Parts Discussed in Thread: ALP
Tool/software:
当使用内部时序和内部时钟生成 pattern 时,如果我将输出设置为红色,为什么输出红色后屏幕颜色突然变黑,然后切换到其他颜色没有任何响应
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90UB947-Q1
Other Parts Discussed in Thread: ALP
Tool/software:
当使用内部时序和内部时钟生成 pattern 时,如果我将输出设置为红色,为什么输出红色后屏幕颜色突然变黑,然后切换到其他颜色没有任何响应
Hi user,
1. What is your hardware setup(deserializer?) and panel resolution?
2. Did you use ALP? https://www.ti.com/tool/ALP We recommend use ALP patgen tab to achieve the patgen function first.

Currently, you can use patgen to output the red, but black screen afterward. It seems to be the PCLK may be mismatch to you panel. Do you have scrip setting or any further information that we can help you.
Regards,
Roy
Hi Roy morning
code as follows
# 947_address:0X10
# 948_address:0X2C
#clock frequency:88.2MHZ
#hactive = <1920>; vactive = <720>; hback-porch = 16; vback-porch = 10; hsync-len = 40;vsync-len = 6;
i2cset -y -f 3 0x10 0x03 0xDA
i2cset -y -f 3 0x10 0x17 0x9E
i2cset -y -f 3 0x10 0x4F 0x80
i2cset -y -f 3 0x2C 0x26 0x16
i2cset -y -f 3 0x2C 0x27 0x16
i2cset -y -f 3 0x10 0x64 0x10
i2cset -y -f 3 0x10 0X66 0X07
i2cset -y -f 3 0x10 0X67 0X80
i2cset -y -f 3 0x10 0X66 0X08
i2cset -y -f 3 0x10 0X67 0X07
i2cset -y -f 3 0x10 0X66 0X09
i2cset -y -f 3 0x10 0X67 0X2D
i2cset -y -f 3 0x10 0X66 0X04
i2cset -y -f 3 0x10 0X67 0X98
i2cset -y -f 3 0x10 0X66 0X05
i2cset -y -f 3 0x10 0X67 0X58
i2cset -y -f 3 0x10 0X66 0X06
i2cset -y -f 3 0x10 0X67 0X46
i2cset -y -f 3 0x10 0X66 0X0C
i2cset -y -f 3 0x10 0X67 0X10
i2cset -y -f 3 0x10 0X66 0x0D
i2cset -y -f 3 0x10 0X67 0x0A
i2cset -y -f 3 0x10 0X66 0x0A
i2cset -y -f 3 0x10 0X67 0x28
i2cset -y -f 3 0x10 0X66 0x0B
i2cset -y -f 3 0x10 0X67 0x06
i2cset -y -f 3 0x10 0X66 0x1a
i2cset -y -f 3 0x10 0X67 0x06
i2cset -y -f 3 0x10 0X66 0x03
i2cset -y -f 3 0x10 0X67 0x53
i2cset -y -f 3 0x10 0X65 0x04
i2cset -y -f 3 0x10 0X64 0x41
Let's say I set the internal timings, and the internal clock outputs red, and the screen colour does turn red, but then the colour fades out.
Hi user,
What is your sync polarity and front porch(total is also ok)? I will give you the sample code for the timing. Or you can follow the app note to build it.
From the command that you provided, the last command is 0x41. it should be green color. So I think the red is not from 947patgen.

Regards,
Roy