This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TS3DV642-Q1: Support CPHY 4 trio ?

Part Number: TS3DV642-Q1

Tool/software:

Dear,

I want to use TS3DV642-Q1 for CPHY 4 trio switch.But,it's seems that there is only 8 data pins including D+ or D-,and CPHY 4 trio will use 12 pins.

So,can I use SCL,SDA, CEC,HPD for CPHY?

Thanks

  • Hi,

    The TS3DV642-Q1 is a 6 differential channel or 12 single ended channel bidirectional multiplexer/demultiplexer. All these channels are functionally equivalent and provides almost identical electrical performance. The channels can be used in an arbitrary fashion for differential and single ended signals in any order. So you can use SCL,SDA, CEC, and HPD for CPHY application.

    Thanks

    David