Part Number: SN65HVD30-EP
Other Parts Discussed in Thread: SN65HVD30, SN65HVD35, SN65HVD32, SN65HVD33
Tool/software:
Hi
I am doing a project that has one master and 60 slave. my MCU is STM32F103 and my data is in UART form. My connection mode is full duplex
and the baudrate is 115200. In each time, my master send a request with ID and that slave responses to it.
At first we connect one slave to RS485 bus and all things was good and system was working. When we connect second slave, the A B differential voltages decreases but connection is still ok. When we connect third slave module to the bus, the bus voltages decreases more then before and now the connection get lost. we used oscilloscope and saw that three data packet is transmitting on A-B but the SN65HVD30 can't verify the data to transmit to the micro (Master's MCU). In other expression, the master request data steel is receiving correct and all three slave see that but the master can't see the responses.
My question is that how we use this IC (SN65HVD30) for Full duplex ???
when a slave don't send a data, we want that the SN65 output be high impedance but this IC is not like this. So how in datasheet is written that this IC is 1/2L and max slave connection is 64 !?
Should we use the SN65HVD35 that is full duplex and has RE DE pins to be high impedance other slave to not driving the bus ?
I tried any change in RT resistor and series resistor and was not responsive. I will thank to anybody that help me.