Part Number: TCAN4550-Q1
Other Parts Discussed in Thread: TCAN4550
Tool/software:
Dears,
My customer use TCAN4550-Q1 in their project. Now customer have two questions:
1.Is there an internal current limit on the CAN line of TCAN4550? What is the maximum current?
2.The customer mainly wants to evaluate: Is it feasible to use the Vccout of TCAN4550 from the anchor point to power CC2642/CC2340? Are there any risks? Does the customer provide specific parameters?
Bluetooth is an application of connect Monitor, and the current is about 10mA.
Many thanks,
Arabella