Part Number: SN65DSI84
Other Parts Discussed in Thread: SN65DSI83EVM
Tool/software:
Hello Team,
We have few follow-up queries as mentioned below.
Could you please help on this as well?
We are planning to use the SN65DSI84ZXHR in our design and have a few software and hardware-related queries for the bring-up and development process:
1. Single-Channel DSI to Two Single-Link LVDS Use Case
We aim to implement a single-channel DSI to two single-link LVDS use case using the SN65DSI84ZXHR. Could you confirm if there are any software limitations or known constraints with this setup? Or can only dual link lvds panels supported (In SN65DSI84 datasheet we referred to Figure 8-1. Typical 1920 x 1200 WUXGA 18-bpp Panel Application)?
Additionally, please provide the required driver files or any reference software available for this chip.
2. SN65DSI83EVM Board Validation
For development, we plan to procure the SN65DSI83EVM evaluation board. Could you share a list of panels validated with this platform, along with any recommendations for compatible panels that have been tested and optimized?
DSI Tuner Software and Validated Configurations
3. Please provide the procedure to download the DSI Tuner software used for configuration.
Additionally, if possible, kindly share validated .dsi configuration files for commonly used panels to expedite the development process.
4. Validation on Qualcomm Processors
Has the SN65DSI84ZXHR been validated on any Qualcomm processors? If yes, please share details on the compatible processors and any available reference designs or implementation notes.
Your prompt assistance with the above queries will greatly help streamline our development efforts.