Part Number: DP83TC814S-Q1
Tool/software:
Hi TI team,
From the SNLA389A – TDR Testing, we can't understand the fault:

1) What's the "Half wire open" and "Peak detect"?
2)0x0310 [5:0]=0x3, it means the fault location in 3m?
Best Regards!
Wang Jingkun
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DP83TC814S-Q1
Tool/software:
Hi TI team,
From the SNLA389A – TDR Testing, we can't understand the fault:

1) What's the "Half wire open" and "Peak detect"?
2)0x0310 [5:0]=0x3, it means the fault location in 3m?
Best Regards!
Wang Jingkun
Hi Wang,
Please note SNLA389B is available on ti.com.
Half wire open is referring to one bus wire being open, as opposed to both bus wires being open. Peak detect is referring to a peak in the signal reflection, which indicates a fault is present on the line.

0x0310 [5:0]=0x3, it means the fault location in 3m?
Correct.
Thanks,
David
Hi David,
1) If both bus wires open, which fault will indicate?
2) Which bit do we read when we test cable diagnosis of TC8? 0x0310 bit [8]? bit [7]? bit [6]?
3) When DUT connects normally and cable is normally, why do we read the cable status is short?

4) When cable is normally, which register can use for indicating the cable status?
Best Regards!
Wang Jingkun
Hi David,
1) If both bus wires open, which fault will indicate?
2) Which bit do we read when we test cable diagnosis of TC8? 0x0310 bit [8]? bit [7]? bit [6]?
3) When DUT connects normally and cable is normally, why do we read the cable status is short?

4) When cable is normally, which register can use for indicating the cable status?
Best Regards!
Wang Jingkun
Hi Jingkun,
Thanks,
David
Hi David,
Link status is given in register 0x1 bit[2]
This is link status. We need to know the status of cable when cable is connected normally.
Best Regards!
Wang Jingkun
Hi Jingkun,
TDR cannot be performed while normal ethernet communication is ongoing. If cable is connected normally, but energy on the line is completely quiet, TDR will show as completed with no fault detected.
Thanks,
David