Part Number: DP83867IS
Tool/software:
Hi Team,
We are having communication problems with the customer system using DP83867IS, and are using the following troubleshooting guide to investigate the cause.
Then, I have a question about section 3.4.
https://www.ti.com/lit/an/snla246c/snla246c.pdf
1) Does it suggest doing steps 1 -> 2 -> 3 -> 4 in that order? Or are these operations independent?
2) Regarding step 4, is the following statement correct?
"Write register 0x01D5 = F508 to change DP83867PHY from low power mode to normal operational mode."
According to the datasheet, I cannot read "low power mode" and "normal operational mode" from register 0x01D5. It seems to be a different register.
Best Regards,