Part Number: TCAN4550
Tool/software:
How much power consumption should I expect while using the TCAN4550 controller in the following mode:
- Test Mode (controller standalone mode): CANH and CANL floating; GPIO1 and GPIO2 are used as RX and TX respectively.
- VIO supplied with 3.3V
- VSUP supplied with Voltage Ranging 6V-12V