Part Number: TCA9539
Other Parts Discussed in Thread: TMS570LS1114
Tool/software:
hello:
I have a question about I2C Fast mode, 400kbps, the specification about of tocf (I2C output fall time- 10-pF to 400-pF Bus), the minimum time is 20*(VCC/5.5V)= 18.18ns@VCC=5V.
Because I had used TMS570LS1114 as the master of I2C, I cannot adjust the I2C sclk output fall time. So the clk output fall time(about 5ns)<18.18ns , it can not fullfill the specification but the circuit works well under this condition. I need the reason why this specification about the minimum time of tocf. If the circuit can not fulfill this specification , what bad condition will the circuit take place ?