Tool/software:
I am referencing the earlier thread as this is the same application. There are a number of photos in the previous thread. I'll repeat one here. In this application the TCA9555 interfaces to Microcontroller TM4C1292NCPDTI3. There is an Analog devices I2C isolator ADUM1250 between the two. The scope screen capture is taken between the controller and the isolator. The pink data trace shows zero levels that are sometimes about a diode drop above ground level. I'm not sure if this is a problem or normal. The I2C lines have 4.7K pull ups to 3.3V on the controller side and 2.2K on the I2Cexpander side. Please comment.
-Dave Lane