Part Number: TCA9803
Tool/software:
Hello,
In TCA9803 datasheet, VOL (Low-level output voltage) is only specified when the input is 0V:
-> Low-level output voltage (VOL) of SDAA and SCLA are specified for VILB =0V.
-> Low-level output voltage (VOL) of SDAB and SCLB are specified for VIA =0V.

Does the Low-level output voltage (VOL) of SDAA and SCLA increase, if VILB is not 0V but 0.3V (for example)?
Does the Low-level output voltage (VOL) of SDAB and SCLB VOL increase, if VIA is not 0V but 0.3V (for example)?
Best Regards
Sylvain