Part Number: DP83869HM
Tool/software:
Hello,
We are Currently using in a new product PHY DP83869HMRGZR
as an SGMII to 10/100 MDI physical layer
i would like to ask for a review about the schemeatics and the magntics connection
as we expreience some issues with the grounds. and sometime DP83869HMRGZR - scheme check.pdf
when connecting the 10/100 ETH1_R/TX_P/N lines without owe have errors while sending and receiveing packages with IPERF testing.
1. when FB7 is connected - we have errors
2. when FB7 is NOT connected - we have errors
3. replaced FB7 with 0Ohm Res - we have errors
Power rails are OK
clock is OK
we do able to send and receive ethernet packages but with errors
plesae advise how to solve - send and receive ethernet packages without errors
Thanks,
Amit