Tool/software:
A customer is facing some issues during development using DP83825I and has some questions.
Q1) During the EMC certification, the PHY LINK is continuously disconnected during the Conducted Susceptibility network 10V test. Are there any solutions or countermeasures?
Q2) During 100Mbps operation, the network environment sometimes drops to 10Mbps. Is this a specification that changes automatically? Are there any registers that need to be set for such behaviour?
Q3) If I want to fix the speed of PHY to 10Mbps, could you please confirm the registers that need to be set and their values?
Q4) Is it correct that I can refer to the value of bit 14 of register 0x10 to check whether MDI or MDIX is operating?
Q5) It seems to be related to the question of Q4, Bit 14 of Register 0x19 is set to force MDI/X. If I change the corresponding pin setting, will the value of Bit 14 of Register 0x10 also change?
Q6) Could you please explain what the Robust_Auto_MDIX feature is?
Q7) Please review the attached circuit below. (Please check if there are any incorrect or parts that need to be modified.)
Schematics (DP83825I, PHY).pdf
Please check. Thank you.