This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83869HM: DP83869HM not initiating any auto negatition pulse and dont see any lights glowing on RJ45 also

Part Number: DP83869HM
Other Parts Discussed in Thread: AM2634, , DP83869, TMDSCNCD263, DP8386X-ASPEED-EVM

Tool/software:

Hi Team,

We have used DP83869HM and AM2634 controller to test ethernet. We have referred of AM2634 PROC_A to design our PCB. We are able to donwload code into AM2634 using JTAG probe.

We are testing ethernet part. So far we have checked below things.

  1. Strap resistor setting for PHY address:

            We have connected same way as AM2634 PROC A schematic. as shown below. Please verify.

2. We have mesured RBIAS voltage:  300mv

3. XI clock input to IC

4. We are providing 1.1V, 2.5V and 3.3V from external power supply. Currently I am manually switching on/off both supplies. We are supplying 1.1V and 2.5V first then within 1 sec 3.3V. Supply

But as per datasheet it shows 2.5 is analog supply and 1.1V should be digital supply. I did not understand this. We are providing both supplies from external power supply

5. DP83869HM IC connections

Both Earth ground and DGND are not shorted

6. We have not programmed any SW in AM2634 yet for Ethernet. Without SW also LEDs should respond

7. MDIO and MDC setting as below

8. We have also changed and mounted new DP83869HM IC. But still not working

Currently, I am stuck with this. Dont have any clue on how to debug futher. This is very important for our project mlestone.

Thanks!