Part Number: TCAN1043A-Q1
Tool/software:
In a previous question it was suggested to use TCAN1044A as a CAN bus activity monitor in order to reduce complexity.
I like the suggestion. Can you review the pin connections to be sure I have this correct.
pin 1 TXD not being used connect to VCC
pin 2 GND connect to system ground
pin 3 VCC connect to 5V regulator ouput
pin 4 RXD connect to LED driver circuit (used to monitor bus activity)
pin 5 NC VIO connect to 5V
pin 6 CAN L connect to CAN L
pin 7 CAN H connect to CAN H
pin 8 STB connect to GND (want to put the IC in receive mode)
Thank you!