Part Number: HD3SS6126
Other Parts Discussed in Thread: HD3SS612, HD3SS3415, HD3SS3212, HD3SS3220,
Tool/software:
Hi TI Team,
Could I use HD3SS6126RUAR to handle the USB-C(type) flip/non-flip states.
Tim
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Tim,
When you mean USB-C type flip/non flip states are you talking about Downward Facing and Upward Facing port operation.
The HD3SS612 ss signal path can support USB 3 data rates 5 or 10Gbps and this is important because usb type c is a just a interface that can operate on USB 3 speeds.
Another device that can support usb c speeds( usb 3 5Gbps or 10 Gbps) is the HD3SS3415 and more info on that can be found on this thread
I believe the better options here that can support UFP and DFP are the HD3SS3212 or HD3SS3220 as this opertion is called out on the datasheets.
Please let me know what you think with this information and I can look into this some more.
Regards,
Kameron
Hi Kameron,
Thanks for your reply,
We have the HD3SS6126 parts in stock, and we want to use it to solve the USB-C type flip/non flip states.
At the same time, We want to confirm whether there will be any unexpected risks in this application, such as the time of switching...
Regards,
Tim
Hi Tim,
Looking into this more the HD3SS6126 alone is not recommended for USB-C type flip/non flip states(UFP and DFP role)
If you want to use the HD3SS6126 in this application you will need to add a redriver to your circuit to handle DFP and UFP( Here is a thread that talks- about this idea)
The best device you can use for this flip/non flip states is the HD3SS3220 as it has a integrated Channel Configuration (CC) logic which helps change the device state to UFP or DFP automatically. This device can automatically handle either type c cable orientation( upside down or right-side up) because of its internal CC controller.
Please let me know if you need any further assistance here
Regards,
Kameron
Hi Kameron,
The redriver is a solution to detect USB-C flip/non flip states.
If there is a PD controller to handle USB plugged-Flip state and notify HD3SS6126 in my system.
What problems does this solution cause?
Regards,
Tim
Hi Tim,
I am not really a expert on PD controllers but your solution using the PD controller and HD3SS6126 looks to be correct.
This design solution is actually talked about on some older e2e threads.
Please let me know if you need any further assistance here
Regards,
Kameron