Part Number: DP83TC812R-Q1
Tool/software:
I plan to set internal delay for 100base T1 RGMII and TX and RX delay shall be set at PHY side.
- If align mode is used during strap setting, and cfg_rgmii_rx_clk_shift_sel=1b cfg_rgmii_tx_clk_shift_sel=1b
what is the RGMII internal delay of TX and RX? only 2 ns? datasheet shows only 2ns.


- If RGMII (TX and RX Internal Delay Mode) is used during strap setting,
What is the RGMII internal delay of TX and RX? 5 ns? because default setting of below register setting:
dll_tx_delay_ctrl_rgmii_sl: 0xFh(5ns);
dll_rx_delay_ctrl_rgmii_sl: 0xFh(5ns);
- cfg_rgmii_rx_clk_shift_sel cfg_rgmii_tx_clk_shift_sel describe if set to 1b then there is 90 degree between clk and data.
- if RGMII align mode used, then the TX and RXD internal delay is 10ns?
- if RGMII (TX and RX Internal Delay Mode) is used, then the TX and RXD internal delay is 15ns?