This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I've got a board which is supposed to be RS485 compatible, but it contains a SN75176a (RS422 part, according to the spec sheet http://www.ti.com/lit/ds/symlink/sn75176a.pdf). I can't seem to find any electrical differences between the "A" and "B" (RS422/485 according to the spec sheet http://www.ti.com/lit/ds/symlink/sn75176b.pdf) versions of the drivers. Am I missing something critical between these two drivers? Is there any reason why the "A" version couldn't be used in a 485 application?
Thanks!
Hello James,
The A and B differ in the switching characteristics (speed). Either device can be used for RS485 because the drive capability is 60mA (for termination at both end of the transmission line).
Regards,
Ron Michallick