Part Number: TUSB522P
Tool/software:
Hi Team
could you help me review SCH as below?
s5406aa_io_r10_TUSB522P_20250307a.pdf
BRs
Brian
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TUSB522P
Tool/software:
Hi Team
could you help me review SCH as below?
s5406aa_io_r10_TUSB522P_20250307a.pdf
BRs
Brian
Hi Brian,
Here is the schematic review:
TUSB522p_Schematic_Review_Pegatron_S5406AA_IO(3_14_2025).pdf
Additionally,
I cannot see the part names for the CMC and the ESD used.
Make sure the CMC has sufficient bandwidth for the 5Gbps data passing through it.
Make sure the ESD is rated for USB3.0, and has a clamping voltage at approx. 5V.
I believe the ESD/ CMC circuitry can be improved. I believe this orientation will be better.