Part Number: DS250DF410EVM
Other Parts Discussed in Thread: USB2ANY, DS250DF410
Tool/software:
Hello TI team,
I would like to connect to the DS250DF410EVM via a separate USB2ANY interface adapter and SigCon Architect so that the SPI lines of the adapter can be run to another device. Then the USB2ANY can be used to configure the SPI device before opening SigCon Architect and configuring the retimer.
What jumper settings are needed to disable the MSP430 on-board the EVM? Does the keyed 10-pin cable from the USB2ANY plug into the connector along the bottom edge of the EVM? I have the User Guide (SNLU203) but it only shows the default jumper settings and does not describe the jumpers functions. Is there anything else I need to consider such as the source of the 3.3V and pull-ups for the SMBus?
Our design will have an MSP430, I2C muxes, LMK clock chip(s) and more than 16 retimers on each board with only one USB connection. We would like to be able to access the different components using USB2ANY and their associated software such as SigCon Architect. It is my understanding that you provide the USB2ANY binary for the MSP430 and an App to flash but do not support it beyond that. Getting a second interface to work through the same USB2ANY that the EVM is attached to is our first step in prototyping this design
Thanks Eric.