Part Number: SN65LVDS100
Other Parts Discussed in Thread: SN65LVDS1, DS25BR100, DS25BR120, DS25BR101
Tool/software:
Good evening,
I want to use an LVDS driver in a custom physical interface, where my input CMOS signal is processed through the pre-emphasis filter. Ideally, the differential output of the LVDS buffer should retain the processed waveform, that is a digital NRZ with the pronounced spikes at the edges. These spikes should be clearly visible and relative in amplitude with the baseline signal on both P and N side, inverted, obviously.
Looking at the input and output circuit of the SN65LVDS1, I see no reason why that wouldn't be the case with this part, but I might be mistaken. Will it work, and if not, which part would behave like that?
Best regards,
P