Part Number: TCA9509
Tool/software:
Hi Team,
As subject , due the A side had the internal current source feature which no needed external pull up on A side,
we would like to ask , in normal operation while the VCCA/VCCB are both valid on device , if we set the "EN" pin as low and turn off the A/B side's driver , is the A-side "current source" still enable?
or the internal current source on A side will also disable while the driver are being disable when EN is low?



Andy