Other Parts Discussed in Thread: DP83869
Tool/software:
hii , I am using DP83869HM phy in my project . i want to make connection between my FPGA AGILEX-7 AND WIFI module. my both phys are sitting between mac and wifi module. I am using it in MII mode 100mbps ,So can i make a direct mdi connection between both PHY's or do i need to add transformer between both. If i can connect directly ,will it function properly or it is mandatory to add transformer. if mandatory then why ?(my both phy are in same voltage level )