Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83822I: Transformer-less Configuration MLT-3 Register Setting

Part Number: DP83822I

Tool/software:

Dear Team,

My customer is considering to use the DP83822I under transformer-less configuration. In case of the transformer-less configuration, writing following extra register to make transmitter of the DP83822I supports the transformer-less application is needed according to below E2E.

Register<0x0404> = 0x0024

DP83822I: Configuration without Magnetics and RJ45

If Register<0x0404> = 0x0020 under the transformer-less configuration, what will happen?

When "0x0020" is specified as reduced MLT-3, while when "0x0024" is specified as full MLT-3, is it possible that the signal amplitude of the MLT-3 is lower than expected in a situation where the value of register 0x0404 is operating at 0x0020 with a transformer-less connection?

Best Regards,

Koshi Ninomiya

  • Hi Ninomiya-san, 

    When "0x0020" is specified as reduced MLT-3, while when "0x0024" is specified as full MLT-3, is it possible that the signal amplitude of the MLT-3 is lower than expected in a situation where the value of register 0x0404 is operating at 0x0020 with a transformer-less connection?

    Yes, this can be true in transformer-less connection so signal integrity can become an issue. Therefore, we suggest customers to use full MLT-3 when they implement transformerless connection. 

    Please let me know if you have any other questions. 

    Best,
    J