Part Number: DS280DF810
Other Parts Discussed in Thread: DS280BR820EVM
Tool/software:
I'm developing a board that takes 100G-KR backplane Ethernet (across four lanes) to a host-side QSFP28 assembly (in other words, the cage and receptacle). I have my eye on the DS280DF810 as a retimer for the signals. There's several points of confusion that I can't find definitive answers on.
- Does the DS280DF810 support conversion from KR to SFI?
- If so, what do I need to do with the DS280DF810 to have it output the correct SFI signal for use with the QSFP28 module?
- What, if anything, do I need to do with the DS280DF810 to allow the QSFP28 assembly to support both direct-attach copper and fiber modules?
I've tried to do my due diligence but it just results in contradictory or inconclusive claims. There's another thread that's similar ("DS280BR820EVM: KR to SFI conversion"), but it simply states "You might also consider DS280DF810" without mentioning to what extent it supports this use case.
Any guidance is appreciated.
Thanks,
Calvin