Part Number: TCA9617A
Other Parts Discussed in Thread: TCA9517, TCA39306, TCA9803, TCA9617B
Tool/software:
Hello, I am currently designing regarding TCA9617A and would like to inquire about the VIL value, especially regarding the B channel.
On DATASHEET, the VIL value of SDAB and SCLB is fixed at 0.4V, but is it fixed at 0.4V regardless of the value of VCCB?
And if correct, why is it fixed differently from SDAA and SCLA?
Since the VOL of the slave IC you're planning to use is higher than 0.4V, it should be checked for compatibility.
And I also used the TCA9517, but it operates based on the VCCA and VCCB supply voltages.