Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] What is a buffered LOW?

Part Number: TCA9517
Other Parts Discussed in Thread: TCA9617B

FAQ: Logic and Voltage Translation >  IxC >> What is a buffered LOW? 

A "buffered LOW" is the output voltage of the buffer when a low voltage input (VIL) is present on the input. 

This buffered LOW is commonly referred to the B-side output voltage when A-side is driven, because it is the B-side that contains the static voltage offset (SVO) present on several I2C buffers - TCA9517 / TCA9517A / TCA9617B.

Given that I2C buffers are bi-directional, inputs and outputs can change reference. *note the direction of the arrows for each pin on the buffer. 

A snippet of the electrical characteristics from the TCA9617B datasheet shows that an input of VILA = 0V will result in an output voltage on B-side VOLB = 0.53 V (typ.) This offset voltage is known as the buffered LOW. 

Here is a oscilloscope example of the buffered LOW voltage when driving the A-side of a buffer with a SVO on B-side.