Other Parts Discussed in Thread: LMH0340, LMH0344, SD307EVK
Tool/software:
Subject: Clarification on LMH0307 for 1:2 or 1:3 HD-SDI Splitter Application
Hello TI Team,
I’m planning to use the LMH0307 as part of a design where I need to split a single HD-SDI signal into multiple outputs (preferably 2 or 3), all with proper 75-ohm drive capability to connect directly to standard SDI monitors or equipment.
According to the datasheet, the LMH0307 accepts a differential SDI input, but in the typical application/reference design, I see a single-ended 75-ohm input being fed to the device. I would like to confirm:
-
Can I provide a single 75-ohm SDI signal (AC-coupled) to the input of the LMH0307 as shown in the reference design and still meet the input requirements of the part?
-
If I use two or three LMH0307 outputs driven from the same SDI input, can I achieve proper SDI fanout (i.e., identical SDI outputs on all channels)?
-
Can the outputs of LMH0307 be connected directly to 75-ohm SDI monitors without any additional driver/buffer stage?
-
Is there any recommended schematic or application note from TI specifically for a 1:2 or 1:3 HD-SDI splitter using LMH0307 or a similar TI part?
My goal is to ensure proper signal integrity across all outputs when splitting a single SDI input, and I would appreciate confirmation on whether LMH0307 suits this use case or if an alternative like LMH0340 or a true fanout buffer would be more appropriate.
Thanks in advance for your support!
Best regards,
Arvind