Part Number: DS125DF410
Tool/software:
Dear Support Team,
Our current product consists of a transceiver device, a receiver device, and the cable that connects them. We are using the DS125DF410 in our receiver device.
The DS125DF410 is used in Manual CTLE mode, and its settings are optimized for Cable A. Currently, we are considering using Cable B instead of Cable A.
Therefore, we need to re-optimize the settings of the DS125DF410 in the receiver device for Cable B. We are considering two methods for optimization:
- Method 1:
Use Adapted CTLE mode.
- Method 2:
Use Adapted CTLE mode in preliminary studies to determine the optimal CTLE settings for Cable B.
Ultimately, we will use Manual CTLE mode and apply the settings confirmed in the preliminary studies.
I am not very familiar with the DS125DF410, so I do not know how to implement these two methods. Therefore, please guide me on how to proceed.
First, is the following approach correct for Method 1? I am unsure whether the CDR Reset via register 0x0A mentioned in steps 3 and 5 is truly necessary.
Additionally, please let me know if there are any other registers I should check or operate on.
- (step 1) Write 0x0C to register 0xFF. (This allows writing to all channels simultaneously.)
- (step 2) Write 0x20 to register 0x31. (This sets all channels to Adapted CTLE mode.)
- (step 3) Write 0x1C to register 0x0A.
- (step 4) Wait for more than 40 usec.
- (step 5) Write 0x18 to register 0x0A.
Next, is the following approach correct for Method 2? Please let me know if there are any other registers I should check or operate on.
(Preliminary study: Set to Adapted CTLE mode and confirm the optimal parameters for Cable B.)
- (step 1) Change our system from Cable A to Cable B.
- (step 2) Write 0x0C to register 0xFF. (This allows writing to all channels simultaneously.)
- (step 3) Write 0x20 to register 0x31. (This sets all channels to Adapted CTLE mode.)
- (step 4) Write 0x1C to register 0x0A.
- (step 5) Wait for more than 40 usec.
- (step 6) Write 0x18 to register 0x0A.
- (step 7) Read register 0x03. (Confirm the optimized CTLE Gain setting value with Adapted CTLE functionality.)
(Final settings: Set to Manual CTLE mode and apply the CTLE Gain value for Cable B obtained from the preliminary study.)
- (step 1) Change our system from Cable A to Cable B.
- (step 2) Write 0x0C to register 0xFF. (This allows writing to all channels simultaneously.)
- (step 3) Write 0x00 to register 0x31. (This sets all channels to Manual CTLE mode.)
- (step 4) Write the setting value confirmed in step 7 of the preliminary study to register 0x03.
- (step 5) Write 0x88 to register 0x2D. (This enables the changes made to register 0x03.)
- (step 6) Set register 0x3A to the same value as register 0x03.
- (step 7) Set register 0x50 to the same value as register 0x03.
- (step 8) Write 0x1C to register 0x0A.
- (step 9) Wait for more than 40 usec.
- (step 10) Write 0x18 to register 0x0A.