Part Number: DP83822I
Tool/software:
Hallo!
When using DP83822 as an EtherCAT PHY and connecting signals between boards, I am considering configuring a circuit using capacitor coupling, referring to the TI document (AN-1519 DP83848 PHYTER Transformerless Ethernet Operation).
Question 1
When connecting boards, should there be only one AC blocking capacitor between the PHYs?
Question 2
Is it okay to connect a capacitor to each of the two PHYs and connect them board-to-board?
Question 3
Is it okay for the capacitance of the two capacitors to be 0.1uF each?
Thank you for your reply.